Cancel
Showing results for 
Search instead for 
Did you mean: 

draft angle in mold design

Creator
Creator
Hello all,
I just want to ask a basic question. How dose NX define whether a face is positive or negative draft when doing the draft analysis or in the check regions( molded part validation)command? Can we say that if the face is invisible when see from the die draw direction, it is negative draft. Otherwise, it is positive draft.
Thank you.

 

2 REPLIES 2

Re: draft angle in mold design

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi ,

I have not used mold design but i guess in fundamental terms your assumption is majorly correct (viewing the part from die direction.) .

It compares the angle between the surface normal and the draw direction you have specified and decides the positive and negetive draft regions.

You can test it using the isocline curves for a rough check on parting line.

Best Regards

Kapil

Re: draft angle in mold design

Creator
Creator

Hi,

Thank you for your suggestions. I will try it now.