Cancel
Showing results for 
Search instead for 
Did you mean: 

drafting visible line not appear

Builder
Builder

Hello experts,

 

i have query in NX 11

 

i have assembly like as attached image ,

 

in that i cant get visible line,

 

i also used silhouettes option ,but not getting solution

 

can anybody help me for this

 

appriciate for help

 

Visible line_currently model like this.JPGassmebly drawingVisible line_not shown.JPGvisible line not showingVisible line_should  be like this.JPGvisible line should show be like this 

Warm Regards
Thomas Roman
Machine Designer
7 REPLIES

Re: drafting visible line not appear

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Thomas_Roman,

Under the section settings, Verify that 'Show background' option is checked.sectionview.png

 

This can also be set in the drafting preferences.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: drafting visible line not appear

Builder
Builder

Hello@Ganesh_Kadole

 

thanks for the reply but not working properly

 

check example for better solution

 

thanks

Warm Regards
Thomas Roman
Machine Designer

Re: drafting visible line not appear

Phenom
Phenom

Make sure you haven't toggled on 'Use Offset' on the Section Line Settings.

offset.jpg

Re: drafting visible line not appear

Builder
Builder

Hello@joewhite,

 

yup the option is activated ,,not getting result

 

 

 

Warm Regards
Thomas Roman
Machine Designer

Re: drafting visible line not appear

Valued Contributor
Valued Contributor
You have to Turn Off the Offset option Smiley Wink

Re: drafting visible line not appear

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
You have to Turn Off the Offset option

Or, make it greater that the body being sectioned for which the silhouettes are missing.  In this case, Example_00102 mirror has a diameter of 90mm.  If you make the offset 45.1mm then the silhouette of that body is shown, but not the hidden lines of the exterior body.

 Screenshot - 8_21_2017 , 9_00_24 AM.png

Docs: Create a Section Line using the Offset Option

"A component or solid body must fall completely within the range of the offset distance before it will appear in the foreground or background of the section view."

 

Regards, Ben

Re: drafting visible line not appear

Builder
Builder
Thanks for the support guys

appreciated for help

thanks again
Warm Regards
Thomas Roman
Machine Designer