Cancel
Showing results for 
Search instead for 
Did you mean: 

edit multiple centerlines

Pioneer
Pioneer

Hello

I`m trying edit multiple centerlines, but cannot find solution.

My workflow

- I created about 20 automatic centerlines for holes

- I edited length of one of them

- I would like to inherit this length to 10 centerlines.

 

Problem is

- When I select more than one centerline, the EDIT is not in the context menu

- When I select one centerline, I can launch EDIT dialog box, but cannot select more than one centerline

- When I select more centerlines, I`m able select SETTINGS. But when I select INHERIT FROM SELECTED OBJECT, the length of the centerlines does not change (because, in Settings dialog is possible change only color and width)

 

Do you have some solution, how to change length of multiple centerlines, or do I have to log ER?

 

Thank you

 

Regards

Martin

3 REPLIES

Re: edit multiple centerlines

Siemens Phenom Siemens Phenom
Siemens Phenom

It is not possible to edit multiple center line symbols at the same time. Please consider filing an ER.

Re: edit multiple centerlines

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@cubalibre00 posted some journal code a while back that edits the length of all the centerlines. It may do what you want, or it may serve as a good starting point for your own customized journal.

 

http://community.plm.automation.siemens.com/t5/NX-Programming-Customization/edit-settings-of-all-cen...

Re: edit multiple centerlines

Pioneer
Pioneer

Hi

 

Sorry for late response, but I`m been on holiday.

Thank you for answer. I expected, that this is for ER, but I need to consult with someone.

Thank you again

Martin