Cancel
Showing results for 
Search instead for 
Did you mean: 

effect of ''Load interpart data''

Creator
Creator

Hello,

 

How do i test the effect of the ''Load interpart data'' on my assembly. I want to know how much time it extra cost to open a large assembly with this funtion activated.

2 REPLIES

Re: effect of ''Load interpart data''

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Luvi,

 

You will have to set your "Load Options" prior to loading your assembly structure. I assume youre controling all your parts in the assembly including the defining parts for the wave linked enities. See the attached image of the options on the "Load Options" menu. Should you want to load the defined linked parts (Interparts Data) you simply toggle the "Load Interpart Data" on. Ensure that your Load options are correct. I assume that you have the correct loadoptions set and thet everything is up to date - if not you will potentially see some updating of parts taking place if you are loading revisions of of parts that is not up to date with the set load options.

 

Best Regards

Fred

Re: effect of ''Load interpart data''

Phenom
Phenom

Hi @Luvi,

depending on how you have created linked geometry. We don't have the license for advanced linked geometry, then linked geometry can be created always with the parent in the assembly structure, so we don't need this option enabled.

If you have geometry linked, but the reference set excludes the parent component, you need to enable the option with 'none' and performance are practically the same.

If you have advanced linked geometry license and you can create linked geometry with one level or more level, you need to enable first level or all level option and the performance can decrease on how many components need to open.

 

Thank you...

Using NX11 and NX1847
RuleDesigner PDM