Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

error in updating NX11 to 11.1

Pioneer
Pioneer

I'm getting a couple of errors while trying to update, I've run it multiple times, I get failed to extract to the filename on 2 files, the rest update OK

 

I am runnuing as administrator and I've checked to make sure I have write access

Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000
36 REPLIES 36

Re: error in updating NX11 to 11.1

Pioneer
Pioneer

It says sharing violation in UGII while trying to move files

 

I just rebooted and tried again, same thing

Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000

Re: error in updating NX11 to 11.1

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Before I assume...

You do NOT have NX running as you try to run the MR?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: error in updating NX11 to 11.1

Pioneer
Pioneer

No, I even did it after a fresh restart just to make sure nothing was locked open

Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000

Re: error in updating NX11 to 11.1

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Are you able to call the GTAC Systems group? They can help you with any installation issues that you're experiencing.

Regards, Ben

Re: error in updating NX11 to 11.1

Pioneer
Pioneer

Yes I can call, I was just wondering is anyone else was getting this and resolved it before I do

 

Thanks

Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000

Re: error in updating NX11 to 11.1

Pioneer
Pioneer

Hi

 

I had the same problem last week installing 11.0.1. I had no other applications running (Win 7) and the install failed with sharing violation. Restarted the computer and installed with not further problems

 

Keith Irvine

Re: error in updating NX11 to 11.1

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
It looks like running update.bat as administrator in safe mode worked in this case.

Regards, Ben

Re: error in updating NX11 to 11.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello i'm getting error 255 while updating to nx11.0 to nx 11.0.1..?

Re: error in updating NX11 to 11.1

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Have you tried opening an NX command window as Administrator, and then running ugs_update.bat in that command window?  There is one case I found where the PATH variable had some questionable entries.  Feel free to post your PATH here so we can check it if you're still having problems.