Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: error in updating NX11 to 11.1

Pioneer
Pioneer

No I did not try this!

Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000

Re: error in updating NX11 to 11.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

I cannot find NX command window on win 10. 

Re: error in updating NX11 to 11.1

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @karthik6,

 

Windows 10 does not show the command prompt option by default, but you can still find it here:
C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Siemens NX 11.0\NX Tools

 

Hope this helps

 

Kind regards,

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: error in updating NX11 to 11.1

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Since I use the command window regularly I now add the NX start menu as a toolbar to the Windows 10 task bar. 

 

Right click on the Windows task bar and select "Toolbars > New Toolbar".

Browse to "C:\Program Data\Microsoft\Windows\Start Menu\Programs\Siemens NX xx.x\" and choose Select Folder. 

This will create a "Siemens NX xx.x" toolbar on the task bar from which you can click on the the ">>" icon and choose "NX Tools > Command Prompt".

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: error in updating NX11 to 11.1

Pioneer
Pioneer

I should clarify my previous reply, I did run update.bat, but I right clicked on it and ran as administrator,  but I did not do it from command prompt. This was what GTAC had me try.

Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000

Re: error in updating NX11 to 11.1

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@karthik6,

 

I just got this error!!  I followed my steps to right click on the NX11 command window and "Run as administrator" and then dragged the NX11.0.1 ugs_update.bat file into the command window.  The update completed successfully.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: error in updating NX11 to 11.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Nce @BenBroad..bt where is this bat file i'm unable to find.can you help me find this

Re: error in updating NX11 to 11.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks @BenBroad I found it

Re: error in updating NX11 to 11.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
and in this window after clicking on instal doc update the same 255 error is poping out

Re: error in updating NX11 to 11.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

and when i'm trying to open help this is the error i'm getting now