02-26-2018 12:30 AM
I ahve NX part with two body (Step files imported from supplier)
Now when i export as STL file they exported as single body, when the stl guys select he wanted them as separate bodies, is there a way i can do that
Solved! Go to Solution.
02-26-2018 04:54 AM
02-26-2018 10:43 AM
Hi Nesthome,
You will have to export the desired bodies to two separate files. Exporting them into one file in one go will make the STL convertion to merge them into one object. The STL guy then have to import the two files and he will have 2 separate enteties in his/her system.
Best Regards
Fred