Cancel
Showing results for 
Search instead for 
Did you mean: 

extend a 3d spline to be perpendicular to a plane

Genius
Genius

I need to extend a 3d spline to be perpendicular to X-Z plane. I know Trim Curve can be used for extending. But I can't find options to set continuity at the plane.

 

ScreenClip [3].png

 

Could you kindly give some clues? Thanks!

3 REPLIES

Re: extend a 3d spline to be perpendicular to a plane

Genius
Genius

Could anybody please give some clues? Thank you!

Re: extend a 3d spline to be perpendicular to a plane

Siemens Phenom Siemens Phenom
Siemens Phenom

I think the best method is to construct a new end to the curve.

 

One method would be to use Bridge Curve. Select the existing curve and slide the start point of the bridge curve to somewhere along the existing one. (Or delete the trim and use the origianl curve end point). As second object change option to Datum and select the plane. Can then modify the setting to get the smoothness of transition you require. Then trim the trimed curve (if not used the original curve) to the start of the bridge curve.

 

Another option would be to create a line perpendigular to the plane then edit the curve end point to be G1 to the line.

 

Steve V

Re: extend a 3d spline to be perpendicular to a plane

Genius
Genius

Hi, @StevenVickers

 

Thank you so much for letting me know that Bridge Curve can do the job!