Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: fail to snap "Intersection"

Genius
Genius

Hi @TimF   Great advice. Thanks!

Highlighted

Re: fail to snap "Intersection"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@TimF wrote:
@surfactant,

No problem - just drill it into your head when you choose the Intersection Point (from the Point dialog's pulldown NOT the Snap Point) that the point will lie on the first object selected of the two.

Sometimes order of selecting objects in NX is VERY important.

When I started on UG, selecting a chain of curves was a bit of an art. I'm glad those days are behind us. But, yes, order of selections can still play a big role in the results.

Re: fail to snap "Intersection"

Genius
Genius

Hi all, I'm still thinking about this issue.

 

In the Point dialog, there's no setting of a tolerance value.

 

Q: How does "Point" > "Intersection Point" decide to create an intersection point sucsessfully (no alert, associative) or unsuccessfully (alert, non-associative)?

 

Thanks!