Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

filter object rules selection

I have a body and a component

The component is in front of the body

I want to select the component but the cursor prefers select the body instead

3 REPLIES

Re: filter object rules selection

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Use the command finder and search for "selection priority"; you can set it to prefer components or bodies or...

Re: filter object rules selection

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

or just stop moving the cursor (mouse) and wait for the quick-pick options dialog to appear, and pick the object you want

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: filter object rules selection

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

You can also add Selection Priority to the Selection Toolbar.  Note also the hot-keys in the Selection Priority drop down.

 

 Screenshot - 6_13_2018 , 1_23_21 PM.png

 

Regards, Ben