Cancel
Showing results for 
Search instead for 
Did you mean: 

ghost line in Sketch Task Environment

Valued Contributor
Valued Contributor

The scene below:

 

  • in sketch task environment of "SKETCH_000"
  • The blue curve is the spline "002".
  • "SKETCH_000" is on the plane of the spline "002".

 

Zooming shows a ghost line under the blue line. It's odd. Why? Thanks!

 

ScreenClip.png

 

ScreenClip [1].png

10 REPLIES

Re: ghost line in Sketch Task Environment

Siemens Phenom Siemens Phenom
Siemens Phenom

After zoom in, In GUI perform RMB > Update Display or Menu > View > Operation > Regenerate Work.

 

Regards,
Ganesh

Re: ghost line in Sketch Task Environment

Valued Contributor
Valued Contributor

Hi @GaneshKadole

 

I only knew "Update Display" is unavailable in Sketch Task Environment. Thanks for letting me know "Regenerate Work" is usable!

 

I can understand the case of two connected lines displayed as be unconnected due to tessellation.

 

I'm still curious about why there are a solid line and a phantom at the position of a single spline object. Maybe this is related to certain NX mechanism of handling splines?

Re: ghost line in Sketch Task Environment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you hover over the line to get the "quick pick" dialog, what does it show?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: ghost line in Sketch Task Environment

Valued Contributor
Valued Contributor

Hi @Ken_A

 

Only one object is there. No "quick pick" dialog. Thanks!

 

ScreenClip [2].png

Re: ghost line in Sketch Task Environment

Gears Phenom Gears Phenom
Gears Phenom

Is that dashed line a constraint indicator?  like a point on line?

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: ghost line in Sketch Task Environment

Valued Contributor
Valued Contributor

Hi @DaveK

 

When the grey reference line is deleted, the ghost line dissappears also! But in the sketch there are only two Conincident contraints on the end points. The ghost line under the blue spline is still difficult to understand.

 

Thanks!

 

ScreenClip.png

Re: ghost line in Sketch Task Environment

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @surfactant,

 

Your reference curve in your sketch is constrainted to the spline, which is outside of the sketch.  I suspect that by constraining your reference curve to the spline, that the sketch needs a copy of the spline in the sketch (the ghost line), in the background the system is likely using the Project Curve sketch command (in fact, if you open your sketch, choose "Project Curve" and select Spline 002, you'll see that the projected curve lies on top of the ghost curve).

 

Hope that helps.

Regards, Ben

Re: ghost line in Sketch Task Environment

Valued Contributor
Valued Contributor

Hi @BenBroad

 

Your guess is very reasonable.

 

Yet as shown below, the projected curve (light blue) lies on top of the spline (dark blue), not the ghost curve (highlighted).

 

Thanks!

 

ScreenClip [1].png

Re: ghost line in Sketch Task Environment

Siemens Phenom Siemens Phenom
Siemens Phenom

(view in My Videos)

The movie doesn't capture me deleting constraints at 01:10 and 01:17.