Cancel
Showing results for 
Search instead for 
Did you mean: 

help tube feature

Builder
Builder

Hi,

Using NX10. I've done a sketch (6) with the intention to do a revolucion of two diametres, Ø1.6 and Ø3. but show up an error. Then I've done one by one, first hole Ø1.6 with tube feature and it's correct. But the second one the same error.  Where are the mistake? 

 

Attached my prt part and pdf with 2D section.

 

Thanks for any help

 

Jose C

3 REPLIES

Re: help tube feature

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @JCP,

I have created the hole feature with the datums and hole feature so that it will be easy to modify/control the diameter and depths. Model is attached.

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: help tube feature

Siemens Phenom Siemens Phenom
Siemens Phenom

It looks like the sketch is coincident with the hole and NX is not sure of your design intent.  

2017-07-05 11_12_56-NX 12.0.0.22 - Modeling.jpg

Moving the sketch slightly means the feature succeeds but I'm not sure of your design intent.

2017-07-05 11_16_16-NX 12.0.0.22 - Modeling.jpg

Re: help tube feature

Builder
Builder
Thanks. Could be ok.

Thanks for your help

Jose C