Cancel
Showing results for 
Search instead for 
Did you mean: 

hide "make unique" in assembly context menu

Genius
Genius

Hello

 

I want to hide the "make unique" command in the assembly context menu. Is this possible via customization in NX10?

 

Thanks in advance

 

Meinolf


Meinolf, , Leistritz Turbinentechnik GmbH


Production: NX10.0.3, TC 10.1.4

Testing:NX11 Beta

1 REPLY

Re: hide "make unique" in assembly context menu

Siemens Phenom Siemens Phenom
Siemens Phenom

There is no practical way to directly modify the contents of a pop-up menu.

 

As you've already noted, you can edit the content of the Short-Cut toolbar as well as the Radial,pop-up but those are the only opportunities that users have.

 

That being said, there actually is a way to indirectly remove the 'Make Unique' option from the pop-up menu but I'm not sure I should be posting this 'hack' on a public website (which the Siemens Community site is).  I would prefer to exchange this sort of information privately via email.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA