Cancel
Showing results for 
Search instead for 
Did you mean: 

import step assembly to the modeling template

Pioneer
Pioneer

Hi everybody

 

I`m trying import STEP assembly, where all components will have attributes from modeling template.I`m able import to existing part, only assembly file, not components

My workflow

- I`ve created new part from modeling template (there are all attributes)

- Then I Imported STEP assembly using FILE-IMPORT-STEP, with option IMPORT TO = WORK PART

- the result is, that attributes from modeling template are only in ASSEMBLY file, not in COMPONENTS

 

Does exist some way, how import all components from STEP assembly to the existing template, or do I need copy attributes between components?

 

Thank you

Martin

 

2 REPLIES

Re: import step assembly to the modeling template

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Martin,

 

Can you please share some picture/image of the same?

When you make the component a DISPLAYED PART are the attributes still missing?

Best Regards

Kapil

Re: import step assembly to the modeling template

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi

In the translator`s directory (UGII_BASE_DIR\STEP203UG) are two *.prt files: step203ugnullnx90_in.prt and step203ugnullnx90_mm.prt. This is template part files for imported step files. So you can replace them, with your own template, and all imported STEP files will have the required settings (attributes, layer categories.....)