Cancel
Showing results for 
Search instead for 
Did you mean: 

kisssoft menu in siemens nx

Experimenter
Experimenter

Hello everyone
I installed kisssoft but I do not see the menu in siemens nx http://www.kisssoft.ch/Manual/en/8984.htm
I also followed the tutorial http://www.kisssoft.ch/Manual/en/8988.htm
but I do not see the kisssoft menu
can someone tell me more
can someone help me
regards

6 REPLIES 6

Re: kisssoft menu in siemens nx

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

in which version of NX are you working?

 

the manual is based on a version before NX9.

The ribbon bar is started in NX9 and here is the menu files also been changed.

 

it is possible that u see the tools by clicking on the menu button.

To get the tools on a ribbon bar u can try to go to customize and see if you can find the tools there.

Check there in the tab commands the menu and classic toolbars.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: kisssoft menu in siemens nx

Experimenter
Experimenter

Thanks for the reply I'm working with nx5 and kisssoft 2011

kisssoft is part of the siemens

there is no one here who uses it ?

Re: kisssoft menu in siemens nx

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would work with Kisssoft.

They should know what they are trying to do, so they *should* know how to fix it.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: kisssoft menu in siemens nx

Gears Phenom Gears Phenom
Gears Phenom
@rugge,

I've installed a few different add-ons from different sources as well as customized NX for 10-15 years and that tutorial is probably one of the least detailed ones I've seen for an addon that is sold to NX users.

I second Ken's suggestion of contacting kisssoft and allowing them to explain the install in more detail to you....it's not just a matter of throwing files in any old location that "users can access at any time" and starting NX. If you have no clue about customizing NX or its environment the chances are quite high that you won't figure it out from their instructions without their help.

The biggest thing I can pass along is to not expect this to run without restarting NX AFTER you've placed all the files in the correct locations and have them correctly defined in the files NX uses to look in those locations.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: kisssoft menu in siemens nx

Experimenter
Experimenter

but my version of 2011 is out of maintenance if I have to ask them, I have to pay them I was hoping there was someone here who used kisssoft

Re: kisssoft menu in siemens nx

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Rugge

just by coincidence stumbled over this old thread. If it is still a topic: you don't need maintenance to ask us, we try to help when ever we can.

So if this is still open, please contact support@KISSsoft.AG.