Cancel
Showing results for 
Search instead for 
Did you mean: 

minimum distance between two curves

Genius
Genius

I want to know whether two curves intersect. Deviation Checking seems to work by creating a sepecified amount of points on the curves and comparing distances between those points.

 

Q1: Is it possible for NX to calulate the minimum distance mathematically?
 
Q2: How can I create the shortest straight line connecting two curves?

 

Thanks!

 

Image.png

4 REPLIES 4

Re: minimum distance between two curves

Gears Phenom Gears Phenom
Gears Phenom

Use Analysis->Measure Distance:

MeasureDistance.png

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.2 MP1]

Re: minimum distance between two curves

Genius
Genius

Hi @Inch   Thank you for the solution!

Re: minimum distance between two curves

Gears Phenom Gears Phenom
Gears Phenom
@surfactant,

As a general practice, I would recommend only using Deviation Checking for situations where faces and/or edges are involved or you require the distance over a span of many points between 2 curves.

I would use Measure Distance for almost everything else, particularly if it's curve to curve and/or Snap Point based.

Just my personal use of the 2 commands - I'm not going to stand on a soapbox and preach to anyone else that feels differently.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: minimum distance between two curves

Genius
Genius

Hi @TimF  I have being thinking about the role of Deviation Checking for a long time. Thank you for sharing your practice!