Cancel
Showing results for 
Search instead for 
Did you mean: 

modeling

is there a way just to copy the outline of a model?

 

4 REPLIES 4

Re: modeling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Something like precise outline? Or are you looking for something else?

Re: modeling

I have a cross section of the part and i just want the out line.

Re: modeling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Create a slice of the model and use precise outline on the slice.

 

Or save the cross section curves and delete the ones you don't want.

Re: modeling

Phenom
Phenom

Use "Intersection Curve" command?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW