Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

multiple cad file converter

Builder
Builder

Hello guys,

 

i have little query in NX,

 

i wanna convert multiple .prt files in .dwg file(autocad file)or other 2d/3d formats,as we required for,

 

is there any provision in NX or by other way to convert

 

appriciate for help.

Warm Regards
Thomas Roman
Machine Designer
4 REPLIES

Re: multiple cad file converter

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, from the Windows Start/All Apps menu scroll down until you find the Siemens NX drop down then select the Dxfdwg option.

Steve V

Re: multiple cad file converter

Builder
Builder

hello StevenVickers

how to convert multiple file via this option

means what is the procedure. for it


thanks

Warm Regards
Thomas Roman
Machine Designer

Re: multiple cad file converter

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Thomas_Roman,

 

  • Start > All Programs > Siemens NX 11.0 > Translators > Dxfdwg
    Note that there are other external translator options available for STEP and IGES
  • Command window opens confirming that your Java version meets requirements - leave this open
  • DXF/DWG Export - NX Data Exchange window opens, choose "Import" or "Export" > Next
  • Under Files to Export, choose the Browse icon and locate the files (Hint: You can multi-select files here)
  • Optional: Under "Files to Create" you can right click the files in the list and choose Rename/Add Prefix/Add Suffix
  • Choose which ACAD file type you require DXF/DWG and hit the lightning bolt icon to complete the translation

Regards, Ben

Re: multiple cad file converter

Builder
Builder
thanks, guys thanks for the support

appreciate for your help
Warm Regards
Thomas Roman
Machine Designer