Cancel
Showing results for 
Search instead for 
Did you mean: 

multple datum planes with section curve

Genius
Genius

How does one create multiple datum planes with the section curve command?

 

For "type", I'm using "Parallel Planes"

 

For "Object to section" I chose all the faces on my object.

 

For "Base Plane" I chose the datum plane at z=0. I get an error message that states  "Modeler Error"

4 REPLIES

Re: multple datum planes with section curve

Siemens Phenom Siemens Phenom
Siemens Phenom

What version of NX are you using and could you at least provide a picture of what you're attempting to do (the actual part file would be better)?

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: multple datum planes with section curve

Honored Contributor
Honored Contributor

Are you dealing with the same part geometry as this thread:

http://community.plm.automation.siemens.com/t5/NX-Design-Discussion-Forum/through-face-does-not-inte...

 

If so, you will need to fix the geometry errors before taking sections.

Re: multple datum planes with section curve

Genius
Genius

JohnRBaker wrote:

What version of NX are you using and could you at least provide a picture of what you're attempting to do (the actual part file would be better)?


I'm using NX10. I'll try and post a pic.

Re: multple datum planes with section curve

Genius
Genius
Thanks for the reply. I'm ignoring that part for now. This would be a general slicing method that I could apply to any part.