Cancel
Showing results for 
Search instead for 
Did you mean: 

not able to add dimensions/ annotation to views in specific Drawing Sheet

Experimenter
Experimenter

Hi All

 

I am not able to add dimensions/ annotation to views in specific Drawing Sheet (In other sheets, i am able to add)

 

While adding dimensions, it is visible in preview but not getting added.

I have tried in nx7.5 &11.

please let me know the option to resolve it.

 

Regards

Santhosh

5 REPLIES 5

Re: not able to add dimensions/ annotation to views in specific Drawing Sheet

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Jasanthoshkumar ,

 

Please attach here a simplified part, if possible?

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: not able to add dimensions/ annotation to views in specific Drawing Sheet

Experimenter
Experimenter

Hi Samadhan

 

I can't upload as it is a confidential data.

But the problem is in few sheets and not entire part

 

Regards

Santhosh

Re: not able to add dimensions/ annotation to views in specific Drawing Sheet

Honored Contributor
Honored Contributor

is the work layer, visible in the drawing sheet?

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: not able to add dimensions/ annotation to views in specific Drawing Sheet

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The first thing that I'd check would be the "layer visible in view" settings. Make sure that your work layer is set to visible in the sheet view that you are working on.

Highlighted

Re: not able to add dimensions/ annotation to views in specific Drawing Sheet

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Jasanthoshkumar 

 

It sounds like your work layer is "invisible in view".

 

Determine your 'work layer' by selecting selecting "Menu > Format > Layer Settings".

Now select "Menu > Format > Layer Visible in View".  With 'Sheet' selected in the list, hit OK and check to see if your work layer shows 'Visible'.  If it doesn't double click the layer and choose OK and then repeat your steps to see if the dimension remains on the sheet (in fact, if the layer was invisible then you'll now see all your dimensions).

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration