Cancel
Showing results for 
Search instead for 
Did you mean: 

nx 9 mold wizard application not showing all material

Pioneer
Pioneer

i am unable to see and assign all available material to part when i start the project in mold wizard application?

only nylon material is listed?

what is the problem?

3 REPLIES

Re: nx 9 mold wizard application not showing all material

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

What NX version are you working on?

 

Did you install the NX Mold Libraies? 

Re: nx 9 mold wizard application not showing all material

Pioneer
Pioneer

i have installed.i want to assign material to part.But since only nylon material is available and no other material like abs etc are available .so how can i resolve this issue?

Re: nx 9 mold wizard application not showing all material

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @rahul83,

 

You only see NYLON because you have not installed the MW Data files which need to be downloaded from the SPLM FTP server.  Once you're logged into the Downloads page these can be found under "NX > Product Updates > Moldwizard".  Download and unzip the data file and install it per the README instructions, including setting MOLDWIZARD_DIR to the correct location.

 

More information can be found in the online documentation.

 

Regards, Ben