Cancel
Showing results for 
Search instead for 
Did you mean: 

nx expression command

Pioneer
Pioneer

Hell Everyone

 

 

Is it possible to import  excell file(which is prepared by us on our dekstop) to the NX by the expression command???

 

 

Can anyone help me about this issue???

1 REPLY 1

Re: nx expression command

Siemens Phenom Siemens Phenom
Siemens Phenom

Do you mean, can I have an expression read the value of a cell in an external spreadsheet?

 

If so, the answer is YES.

 

When in the expression dialog, while creating an expression and it comes to assigning the value or 'Formula' for the expression, select the [i][b]f(x)[/b][/i] icon at the bottom of the expression dialog and then select the 'Category' titled 'Spreadsheet' and you'll see a series of functions which will allow you look for and read values for individual cells of an external spreadsheet as well as create list expressions from a range of cells.

 

 

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA