Cancel
Showing results for 
Search instead for 
Did you mean: 

plotting an area of the current display

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

hello,

is it possible to plot only a selected area of the current display, with a controlled scale?

Thank you for any good tips!

5 REPLIES 5

Re: plotting an area of the current display

Honored Contributor
Honored Contributor

Using Plot, you should be able to make sure it's set to "current display", and what is on the screen will be plotted.  As long as the scale is set to 1:1, it should plot that way.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: plotting an area of the current display

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

thank you Dave, but I need to plot a selected area, which doesn't correspond to what I can get with the "current display" option (it often has a different ratio); I would like to set the printing area by dragging a rectangle. To my knowledge it is not possible, but maybe there is some advanced option that I don't know...

Re: plotting an area of the current display

Honored Contributor
Honored Contributor

Other than changing the display window size, I'm not aware of a way to do that.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: plotting an area of the current display

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

This is anyway a good tip, thank you I will try!

Re: plotting an area of the current display

Experimenter
Experimenter

I appreciate that I'm a little behind in this conversation but the SDI BPS plotting solution allows you to plot a viewport while maintaining scale.
Do this with the Advanced Plot option to launch our interface and then the CGM Viewer - Right-Click the drawing to select the desired viewport:

bps1.pngviewer.png

WIth a viewport selected, you can plot just the data you're interested in.

 

Regards,

 

Guy