02-01-2018 01:12 AM - edited 02-01-2018 01:13 AM
Solved! Go to Solution.
02-01-2018 05:38 AM
Hello,
'Pattern Geometry' is creating the Associative output points.
Thanks,
Mathi K
02-01-2018 05:45 AM
So far as i tested it wasn't possible to set a correct and point that is furture dan 100%.
See movie for a work around
02-01-2018 06:31 AM - edited 02-01-2018 09:31 PM
Hi @surfactant
I added one more step.
1. Create Datum Axis with 2 point ( green point and csys orign).
2. When define sketch for the circle,
Specify Horizonal direction with Datum Axis (Step1)
The circle start point is same with horizontal direction.
02-01-2018 07:39 AM
Hi @SKAHN Thanks! I can't understand your solution well. But I tried it roughly in sketch. I still can't see how NX decides the start position on a circle.
Hi @ruud_vandenbrand Thanks for the video! But the solution seems to be too complicated.
Hi @MATHI_CAX_TRG Thanks!
02-01-2018 12:41 PM
Hi @surfactant,
So the requirement is to create a circle, given a specific start point, and create a point set based on that start point? Using the following, if the start point moves the start of the circle moves, and hence the point set (not sure if this is what you're looking for). Otherwise, use @MATHI_CAX_TRG suggestion - Pattern Geometry, or Pattern Feature.
Regards, Ben
02-01-2018 10:12 PM