Cancel
Showing results for 
Search instead for 
Did you mean: 

problem with step and iges files

Experimenter
Experimenter

Hello,

a friend of mine drew a simple component using Catia. He gave me the files of this component in .stp and .iges format. When I try to open the files with NX in .step format I obtain the error: "Library not found", while when I try to open the file in .iges format the following message is displayed: "It is impossible to find or to load the library of the IGES' converter. Install the optional Kit for .iges".

What should I do? 

3 REPLIES

Re: problem with step and iges files

Siemens Phenom Siemens Phenom
Siemens Phenom

If you have the licenses for the translators then it would seem that there might have been a problem with the install.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: problem with step and iges files

Siemens Phenom Siemens Phenom
Siemens Phenom

Was NX installed using the "Quick Install" or "Typical Install" option?  It could just be that the Translators were not installed when NX was originally installed.  You can check by running the Siemens NX 11.0 InstallShield Wizard and choose "Modify".  When you hit "Next" you'll see which features are installed, one of which is "Translators".

Regards, Ben

Re: problem with step and iges files

Experimenter
Experimenter

Thak you all. Tha Translator was only not installed.