Cancel
Showing results for 
Search instead for 
Did you mean: 

"Import files for Part" message upon save

Honored Contributor
Honored Contributor

I have a user, that is getting the following message, when he saves.  I asked if he was importing anything, and they siad no, and said no importing at all in this NX session.

 

any thoughts?

ImportFilesForPart.jpg

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10
13 REPLIES 13

Re: "Import files for Part" message upon save

Honored Contributor
Honored Contributor

Tracked down this "default.log".  Appears to me, that this is studio material related?

 

----------------------------------------------------------------------------------------------------
Model to Translate:   @DB/237688/01.prt
Location of Model :   UGMGR
Config File Path:   \\ncentfilsrv02\NX_Files\NX\NX110custom_ProdDB\NX110library\NX110tess.config
Translator version:   NX 11.0.2
Translation Began on:   Fri Feb 16 13:28:30 2018

----------------------------------------------------------------------------------------------------

version "EAITranslator" 1.0.0 "EAITranslator"
EAITranslator {
	OutputDirectory = ""
	CommonPartsPath = ""
	chordalOption = "RELATIVE"
	structureOption = "MIMIC"
	writeWhichFiles = JTPARTS,JTASSEMBLY
	pmiOption = "PART_AND_ASM"
	JtFileFormat = "9"
	triStripOpt = true
	seamSewing = false
	seamSewingTol = 0.001
	includeBrep = true
	autoNameSanitize = true
	updateChangedPartsOnly = false
	verboseReporting = false
	writeAsciiAssembly = false
	singlePartsNoAssem = false
	autoLowLODgeneration = true
	smartLODgeneration = false
	numLODs = 3
}
Filter {
}
Metadata {
}
LOD "1" {
	Level = 1
	Chordal = 0.001
	Angular = 20
	Length = 0
	AdvCompressionLevel = 0
}
LOD "2" {
	Level = 2
	Chordal = 0.0035
	Angular = 0
	Length = 0
	FeatureSuppression = 0
	Simplify = 0.4
	AdvCompressionLevel = 0.5
}
LOD "3" {
	Level = 3
	Chordal = 0.01
	Angular = 0
	Length = 0
	FeatureSuppression = 0
	Simplify = 0.1
	AdvCompressionLevel = 1
}
ugConfig {
	doWireframe = false
	mergeSheets = true
	mergeSolids = false
	checkLayers = false
	XTbrep = true
	appendRefSetName = false
	getAttributes = true
	representAttributesAs = "DEFAULT"
	getNXBodyNames = false
	appendItemName = true
	appendRevision = true
	excludeViaRefSet = false
	usePreferredRefSets = false
	spotWeldSize = 1
	activateCsysPMI = true
	activateDimPMI = true
	activateGDTPMI = true
	activateNotePMI = true
	activateSymbolPMI = true
	activateSupplementalGeomPMI = true
	activateWeldPMI = true
	activateWeldLabels = true
	activateMpawPMI = true
	applyPMIRefset = true
	configureLeafNodeName = false
	configureFileName = false
	includeInvisible = true
	LogReporting = "ERROR,WARNING,INFO"
	ConsoleReporting = "NONE"
	LogFileName = "UG_PART"
	useRefsets = "DEFAULT"
	getCADProperties = "CAD_DENSITY,CAD_MATERIAL,CAD_MASS"
	advancedMaterials = true
	doSectionViews = true
	activateFilters = "LAYER"
}
/////////////////////////////////////////
Processing Model  :@DB/237688/01
Process :Starting Translation Session
/////////////////////////////////////////
WARNING 2556 :Translation process has detected doSectionViews option in the configuration file. This option is renamed as LegacyHeavyweightSectionViews. Please set LegacyHeavyweightSectionViews = true in the configuration file to write legacy PMI section views in to a JT file.

WARNING 2558 :This translation has detected advancedMaterials = true in configuration file. NX do not have access to NX STUDIO license required to process NX textures. The translation will continue with advancedMaterials = false settings.

INFO 3610 :About to export data for component - mode is [4]

/////////////////////////////////////////
Processing Model  :@DB/237688/01
Process :End of Translation Session
/////////////////////////////////////////

----------------------------------------------------------------------------------------------------
Total No of Reported Messages to Log File   : 3
Last Node where Error Occurred              : NONE
Total Time to Export           : 0secs
----------------------------------------------------------------------------------------------------
-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: "Import files for Part" message upon save

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

It's a log file resulting from the creation of JT data.

 

It looks like the NX part has geometry and properties that are failing to translate to JT due to an option being disabled, and the lack of a license.

 

Regards, Ben

Re: "Import files for Part" message upon save

Honored Contributor
Honored Contributor

I'm trying to log an IR on it, but now our sold-to is being rejected as "invalid".

 

part cleanup doesn't help.  Any thoughts on what has been disabled?

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: "Import files for Part" message upon save

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Did the user complete a "File > Export > JT" during the session, or do they just have Save JT Data enabled in the Save Options?

 

Based on these two warnings: 

WARNING 2556 :Translation process has detected doSectionViews option in the configuration file. This option is renamed as LegacyHeavyweightSectionViews. Please set LegacyHeavyweightSectionViews = true in the configuration file to write legacy PMI section views in to a JT file.

WARNING 2558 :This translation has detected advancedMaterials = true in configuration file. NX do not have access to NX STUDIO license required to process NX textures. The translation will continue with advancedMaterials = false settings.

 

For Warning 2556 - edit your tessUG.config file (%UGII_BASE_DIR%\PVTRANS) and add LegacyHeavyweightSectionViews = true under the ugConfig section. 

 

For Warning 2558 - It appears your part has textures applied to it and although your tessUG.config file has advancedMaterials = true this session did not have access to an NX STUDIO license required to translate the textures to the JT file.

 

Does that help?

Ben

Re: "Import files for Part" message upon save

Honored Contributor
Honored Contributor

One last question @BenBroad  If we edit tessUG.config for this user, is there a way to do it company wide?  I'm not sure if any others will have this issue, and I hate to make local edits, and have an update over write it.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: "Import files for Part" message upon save

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

The ugii_env_ug.dat file has the following:

 

############################################################################
#
#  PVTRANSUI
#
# PVTRANSUI_DIR points to the directory containing pvtransui application
#
PVTRANSUI_DIR=${UGII_BASE_DIR}\pvtrans
#

Re: "Import files for Part" message upon save

Honored Contributor
Honored Contributor

The NX110env.dat file from NXcustom doesn't, I wonder if it is buried in another file.

 

FYI, we do save JT upon save.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: "Import files for Part" message upon save

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

To point to a network version of the tessUG.config file you can set the following variable:

 

UGII_PV_TESS_CONFIG_FILE

 

Overriding the default JT configuration file

 

Regards, Ben

Re: "Import files for Part" message upon save

Honored Contributor
Honored Contributor

OK, added LegacyHeavyweightSectionViews = true to the NX110tess.config file, in NXcustom.

 

Edit, UGII_PV_TESS_CONFIG_FILE was already set to a server location.

 

 

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10