Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: "Import files for Part" message upon save

Honored Contributor
Honored Contributor

User restarted NX, and is still getting the WARNING 2556 error/warning.

 

I started a new NX ssession, and looked in the log file, and see no mention of "LegacyHeavyweightSectionViews = true", would it show here?

 

 

 

 

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: "Import files for Part" message upon save

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Looks like there may be an additional setting you need to add to the tessUG.config file:

 

Section views in JT files

 

NX to JT translator writes the section view to the JT file only when you:

  • Generate a JT file using File tab→ExportJT or command line application ugtopv invoked with -honour_structure option.

  • Set LegacyHeavyweightSectionViews = true and mergeSolids = true in the JT configuration file.

    Note

    The LegacyHeavyweightSectionViews option is not available in the default JT configuration file shipped with NX. You have to include it in your tessellation configuration file.

Re: "Import files for Part" message upon save

Honored Contributor
Honored Contributor

Changes made, waiting on user to restart NX and test.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: "Import files for Part" message upon save

Genius
Genius

We had a similar problem but cleared it by deleting the default.log file from the item folder in the temp folder. This is covered in PR8340533 on the GTAC solution centre.

Mike

NX 12.0.0 TC11.3 VMU 11.3