Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

"Publish Technical Data Package" NX1847

Legend
Legend

Hello,

 

in NX1847 it should be possible to create a "Technical Data Package". This is what the documentation says.

I am not able to try that, since this command is not available. I am using this License bundle: NX13300N

 

Does anyone know how that works?

 

Thanks!

Regards,

Thomas

17 REPLIES 17

Re: "Publish Technical Data Package" NX1874

Genius
Genius

An additional licence is required for TDP. This is not included in the Mach 3 bundle.

Mike

NX 12.0.0 TC11.3 VMU 11.3

Re: "Publish Technical Data Package" NX1874

Legend
Legend

Thank´s Mike!

 

I was afraid to hear that :-)

 

Thomas

Re: "Publish Technical Data Package" NX1874

Genius
Genius

I checked the beta licence we had and there is a feature in there called nx_tdp which you will require.

 

If you get a licence then ensure you set the customer defaults to point to the folder containing your templates.

 

Mike

NX 12.0.0 TC11.3 VMU 11.3

Re: "Publish Technical Data Package" NX1874

Siemens Phenom Siemens Phenom
Siemens Phenom

@TomK76,

In post  title and description, it should be NX1847...not NX1874 Smiley Surprised 

Re: "Publish Technical Data Package" NX1874

Legend
Legend

@GaneshKadole 

 

Thanks :-)

 

sorry for that! I will call it just NX in the future ;-)

 

Best regards,

Thomas

Re: "Publish Technical Data Package" NX1874

Phenom
Phenom

That is very unfortunate.  I wish this licenese information is included into the "Blogs" when being released into the forums, so we would know if this is included in the 3D PMI package or it would a completly new lincese.  I was under the assumption that this would be part of the 3D PMI license.  

 

Thanks


Shane

 

 

Re: "Publish Technical Data Package" NX1874

Legend
Legend

@sdeters  I agree, this information would be useful.

In general it is sometimes not easy to figure out what functionality requires what license.

 

Thomas

Re: "Publish Technical Data Package" NX1874

Gears Phenom Gears Phenom
Gears Phenom
@sdeters,

In general, it would be nice to know anything about required new licenses or what products are included in bundles without having to pick up the phone. It's almost 2020 and I still have to call someone to find out what bundle contains specific products or if additional licensing is needed for a new product.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.7

Re: "Publish Technical Data Package" NX1874

Honored Contributor
Honored Contributor

Agreed.  What is so proprietary, about a list/matrix of which license bundles allow what functions?

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10