Cancel
Showing results for 
Search instead for 
Did you mean: 

"distribution annotation" command is disabled?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello everyone!

 

Why "distribution annotation" command is disabled?? Are you able to help me?

 

 

 

Bez tytułuadnot.png

 

Best regards

Lukipap

3 REPLIES 3

Re: "distribution annotation" command is disabled?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @lukipap,

 

It could be that you're not licensed for that command.  Distribute Annotations checks out the 'nx_drawing_auto' module, so check your license file to see if that module is included.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: "distribution annotation" command is disabled?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
but it is working on NX 10 and it isn't on NX 11. I have one license for both.

Re: "distribution annotation" command is disabled?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would look at the license server log file for NX10 & Nx11 & see what feature(s) it is attempting to check out.

Then compare to the features in the license.

Then ask your sales rep/VAR why the difference...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled