Cancel
Showing results for 
Search instead for 
Did you mean: 

realize shape and subdivision modeling in NX9

Pioneer
Pioneer

Hi, maybe a stupid question but, is realize shape for subdivision and box/cage modeling in nx 9, part of the seperate module ? can not find any of the commands and menus

10 REPLIES 10

Re: realize shape and subdivision modeling in NX9

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Have you tried command finder?

Ben

Re: realize shape and subdivision modeling in NX9

Pioneer
Pioneer

yes I did.. tried ...realise shape...

Re: realize shape and subdivision modeling in NX9

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Try "realize"

Re: realize shape and subdivision modeling in NX9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"Realize shape" is not part of the basic bundle. It is part of a high end bundle (mach 3?) or you can get it as an add-on bundle. At least this is how it was a year or so ago when we looked into it.

 

If you have a license (or think you may) look on the "Surface" tab for the "Realize shape" icon. If you have a license it will launch you into a separate environment, similar to working with a sketch in the "sketch task environment".

Re: realize shape and subdivision modeling in NX9

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

I see it in NX9.0.2 help docs. Which maintenance release of NX9 do you have installed?

Also in NX9.0.1 What's new, so it may not have been in the base release NX9.0.0, if that's what you have installed.

 

Regards, Ben

Re: realize shape and subdivision modeling in NX9

Pioneer
Pioneer
I have been told that I have a mach 3 version

Re: realize shape and subdivision modeling in NX9

Gears Phenom Gears Phenom
Gears Phenom

There are various types of MACH3 licenses bundle:

I know

 

NX13100

NX13200

NX13300 (my license)

 

only NX13100 and NX13300 has SHAPE STUDIO application.

 

Ciao

 

Re: realize shape and subdivision modeling in NX9

Pioneer
Pioneer
  1. I actually have this license bundle nx13300n..  but still can not find this fonction. :-S

Re: realize shape and subdivision modeling in NX9

Honored Contributor
Honored Contributor

Check your role, change to "advanced", in case your current role has the command hidden.  I thought the command finder would list it, even if hidden though, and say in the comments that it is hidden, etc..

 

RealizeShape.JPG

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10