Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: refining curve: degree vs. segments

Gears Phenom Gears Phenom
Gears Phenom

@surfactant,

What's the endgame - Class A, G1 only, up to G2???? What will this spline be used for - a planar surface? Would a line work better?

Knowing all of that helps to determine which of the above splines would be preferred/acceptable, if it's even needed.

 

Not sure what you gain using a spline to control shape if it's planar. Smiley Wink

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6
Highlighted

Re: refining curve: degree vs. segments

Genius
Genius

Hi @TimF   Thanks! The curve is to be used as an internal controlling curve for a class A surface. Generally in my project I often need to fill a large openning with only several boudary curves. As taught in many previous threads, I try my best to improve and check the quality of those input curves.