Cancel
Showing results for 
Search instead for 
Did you mean: 

retain automatically in clone assembly

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Is it possible?

We have this assembly structure:
Assy
AAAA1
AAAA2
BBBB1

BBBB2

We would like to clone the assembly, but there is no need to clon components which are named "BBBBX".

We wouldn't like to set manually the retain setting in the clone menu. On the contrary, we are looking for an atributte which can set to some of the components to mark as "retained". Something like 'Clone_Retained=YES'...

 

 

Thank in advance,

 

 

 

3 REPLIES

Re: retain automatically in clone assembly

Phenom
Phenom

I don’t expect much from Clone command. Basically it’s unable even to identify Master model drawings of a project.

You have to go through a lot of workarounds and manual inputs to get any work done.

Very primitive and limited functionality compared to other software.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: retain automatically in clone assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @fsh27,

 

The ability to assign an attribute to prevent a part from being cloned was requested in ER 6557212.

 

Regards, Ben

 

 

Highlighted

Re: retain automatically in clone assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would first get yourself added to the mentioned ER by GTAC.

Until this is implemented, you should be able to use a clone notify callback to set the default clone action.

Sorry, no source code, didn't need it by now.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide