Cancel
Showing results for 
Search instead for 
Did you mean: 

reusable object with infinite lenght

Pioneer
Pioneer

I am trying to build a reusable object, a kurt master tumbstone with 4 sides with double jaws... I am trying to get a spreadsheet that would let me decide whatever jaw opening I want when I import my wise form the reusable library...I am trying to find an example of a spreadsheet that let me enter a precise dimension... instead of a pre-define jaw opening dimensions... any clues on how to acheive that ? Right now my jaws opening are constraint with a dimension related to a user expression... thanks...

3 REPLIES

Re: reusable object with infinite lenght

Phenom
Phenom

Use an excamation mark ! infront of the parameter name.

user_input.jpguser_edit.jpg

Re: reusable object with infinite lenght

Pioneer
Pioneer

thanks it worked. Now let push it a little further... How can I have my wise to have options with different jaws size or step jaws or custom jaws...  that I would be able to also select while I am importing my wise..

Re: reusable object with infinite lenght

Phenom
Phenom

You would have to model each jaw option in the file and create an expression to control the suppression of the Feature.

Edit Feature --> Suppress by Expression ( using 1 or 0)

Include the expression in the excel sheet.

 

Not sure why you are going down the path of Reusable Object which is an import, I think I would be creating an Assembly with Arrangements.