Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

review measured distance

Genius
Genius
In the picture below, "SKETCH_000" has a line (highlighted) of the length from measured distance between the ends of "Arc (1)". Sometimes I need go back to check the measured objects of "projected_dist24".
 
How can I manage the measured expression "projected_dist24", which is not listed under the node "Measures"? Thanks!
 
ScreenClip [2].png
2 REPLIES 2

Re: review measured distance

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @surfactant,

After arc, Measure the required distance with associative option toggled on so that this measurement will be listed under the 'Measures' and 'Model History' folder. Then use this measurement expression to define the length of line in sketch.

 

EXP1.png

 

Re: review measured distance

Genius
Genius

Hi @GaneshKadole

 

So, in other words, to make the later maintenance easier, in-command measurement should be avoided. Thanks!