Cancel
Showing results for 
Search instead for 
Did you mean: 

severe bug at modifying and leaving a sketch

Valued Contributor
Valued Contributor

Dear community,

 

I experienced a really annoying bug a few times already.

Does anybody of you know this bug as well?

What is the reason for that behavior?

 

I work with assemblies, components and links. I want to modify a sketch, e.g. a dimension. Then I want to leave the sketch by pressing the "Finish Sketch" button. In this moment I just see that my dimension modified turns back to its old value and I am still in the sketch.

I have to press "Finish Sketch" a few times to make NG leave the sketch. My Dimension has still the old value.

I really have to leave NG completely, closing all my parts and restatring everything again,

 

After that I can modify my sketch and also "Finish Sketch" button works properly.

 

Many thanks for your help.

 

NX 10.0.3.5

NX Phase 5

NX Patch NX 10.0.3.5 MP10, 11Oct16

 

 

 

 

1 REPLY 1
Highlighted

Re: severe bug at modifying and leaving a sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sounds like something that should be reported to GTAC (directly or thru your reseller).

Next time it happens, save a copy of your syslog (File -> Help -> Log file)

You might also try running "part cleanup" (File -> Utilities -> part cleanup)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled