Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

shortcut keys always reset automatically

Experimenter
Experimenter

i have problem in nx that always i set shortcut keys and dont know how in day or in month , nx is reseting can any one fix this problem 

4 REPLIES 4

Re: shortcut keys always reset automatically

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Sayedshahed,

Did you save role after defining shortcut?

Make sure that you are using same role when shortcut was defined.

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: shortcut keys always reset automatically

Honored Contributor
Honored Contributor

I had one user, that set a lot of keyboard shortcuts, and every so often they would stop working.  We found his user.mtx would not fully save, or became curruprted.  essentially it was cropped, and the keyboard short cuts were not in the file.  Once this happened, the file would not save again, and remained in this shortened currupt state.

 

I would take a look at your user.mtx, and make sure it is all there.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: shortcut keys always reset automatically

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Like others suggested, have the user set up all their shortcuts, then save a role.

If the shortcuts "disappear", have them reload the role.

 

Note if they make other UI changes (add/re-arrange icons/tabs/etc.) they should save another role.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: shortcut keys always reset automatically

Experimenter
Experimenter
thanks ganesh