Cancel
Showing results for 
Search instead for 
Did you mean: 

sketch color

Genius
Genius

Hello,

I'm working on a drawing that someone else created and am fighting what should be a simple sketch issue.  I'm trying to draw a simple rectangle, so I activated sketch on the view.  I then created a rectangle, but only the dimensions show up. The actual sketched lines do not show on screen.  Is this just a settings issue or something?  Related to this, is there also a setting that I can change so that the dimensions in the sketch don't stay displayed after I exit the sketch?  I've been hiding them, but it seems like there should be a setting so that they are hidden after I exit out of the sketch.  Thanks

2 REPLIES

Re: sketch color

Siemens Genius Siemens Genius
Siemens Genius

Have you checked the visible in view settings for the view you are trying to work on? 

The sketch geometry colors?

Re: sketch color

Genius
Genius

That fixed it.  The sketch geometry colors were correct, but the previous person had a different layer set.  I changed the work layer and the sketch displayed.  Thanks