02-04-2016 04:14 AM - edited 02-04-2016 08:15 AM
Hi everyone,
I came across a error saying that loop is open and sketch is not valid.
Ho can I find the disconnected points? Is there a way to automatically fix that by adding coincident constraint when two points is within a proximity tolerance?
Thank you!
Solved! Go to Solution.
02-04-2016 05:36 AM
Hi,
Yes you can use AUTO CONSTRAIN for that (in SETTINGS use a distance tolerance value greater than the gap...but it should not be used for closing large gaps (as it might change the sketch if it is underconstrained).
Best Regards
Kapil
02-04-2016 08:14 AM
It works!
Thank you!