Cancel
Showing results for 
Search instead for 
Did you mean: 

[solved] how to do box selection of line ends and circle centers in sketch

Pioneer
Pioneer

Hi everyone,

Box selection of points including line end is useful for adding coincident constraint, but it does not work if one of the point is a line end or start, is there a setting to enable treating line ends like seperate point so it can be selected using box selection?

Thank you!

2 REPLIES

Re: how to do box selection of line ends and circle centers in sketch

Siemens Phenom Siemens Phenom
Siemens Phenom

There is no current setting to treat the end of a line like a point during rectangle selection.

 

The only method would be to manually create a point entity on the ends of the lines.

Re: how to do box selection of line ends and circle centers in sketch

Pioneer
Pioneer
Good to know. Thank you!