Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

split curve by knots, with associativity?

Genius
Genius
Sometimes I want to use a segment of a multi-segment spline.

 

Since Divide Curve > At Knot Point would lose parameters of the input curve, generally I work in this way:

 

  • create a Point Set > Knot Points
  • create a construction line between two knots
  • select the segment by Stop at Intersection

 

Is there a better way to do the job while keeping associativity? Thanks!

2 REPLIES 2

Re: split curve by knots, with associativity?

Gears Phenom Gears Phenom
Gears Phenom
@surfactant,

Trim Curve can use points as boundaries for trimming and you have the option of making it associative.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: split curve by knots, with associativity?

Genius
Genius

Hi @TimF   It works. Thank you for the solution!

 

In Fit Curve, NX automatically segments a complex curve. This automatic segmentation scheme seems to be much better than manual visual judgement as I described in a previous thread. That's why I tried to divide a curve by knots.