Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

the data can't open in Nx 7.5, Nx 8, Nx 9, Nx10, Nx11 or Nx 12

This data was created in 1997, I tried to open in Nx 7.5, 8, 9, 10, 11 or 12. but I can't open it. Which version can use I for opening it?

4 REPLIES 4

Re: the data can't open in Nx 7.5, Nx 8, Nx 9, Nx10, Nx11 or Nx 12

Siemens Phenom Siemens Phenom
Siemens Phenom

NX does not recognize this as a valid part file so you won't be able to open it in any version. Although it has a .prt extention, it either was never an NX part file, or somehow became corrupt and is missing the necessary information for NX to open it. 

 

Generally speaking, any version of NX should be able to open a part last saved in any previous versions going back to Unigraphics.

Regards,
Abe

Re: the data can't open in Nx 7.5, Nx 8, Nx 9, Nx10, Nx11 or Nx 12

Thank you Abe Smiley Happy

Re: the data can't open in Nx 7.5, Nx 8, Nx 9, Nx10, Nx11 or Nx 12

Legend
Legend

Maybe it's Pro/e or SDRC Ideas?

 

They both use the .prt extension.

 

 

Or maybe CadKey? 

https://www.kubotek3d.com/blog/prt-the-legacy-3d-cad-format

 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: the data can't open in Nx 7.5, Nx 8, Nx 9, Nx10, Nx11 or Nx 12

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

I concur with @R_Newcomb - it appears to be a CADKEY file.

 

You can download a free viewer from Kubotec 3D to verify this and while they have a free 15 day trial for their CAD product it does not include the translators that you would need to use in order to get the data into NX.

 

Regards, Ben