Cancel
Showing results for 
Search instead for 
Did you mean: 

trim in direct model

Creator
Creator

Hello, how i can trim in direct modeling like skech, and make fillets , the tools in direct model are so poor...you can see rhino program work..thx

5 REPLIES 5

Re: trim in direct model

Siemens Phenom Siemens Phenom
Siemens Phenom

If you want to trim and create fillet in sketch then there are commands available for it. Edit sketch and look for command Fillet and Quick Trim. You can also use shortcut keys to start command. F for Fillet and T for Quick Trim.

Re: trim in direct model

Creator
Creator
i wan´t use skech , i do it in direct modeling

Re: trim in direct model

Gears Phenom Gears Phenom
Gears Phenom
Please give an example of what you want to do and we will try point you to the command that might do the trick.

More than likely you're not going to be able to do EVERYTHING you want to do using only Direct Modeling commands - that was never the intent of Direct Modeling when it was added to NX. It is a COMPLIMENT to the existing modeling commands within NX.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: trim in direct model

Creator
Creator
see my video

Re: trim in direct model

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What video?

I don't see any links or attachments in *this* thread

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled