Cancel
Showing results for 
Search instead for 
Did you mean: 

turn off point coordinates en nx 75

Valued Contributor
Valued Contributor
Hi everyone, Do you know if its possible to "turn off" point coordinate data when editing curve parameters (among other comands)? Find attached two images, one in NX75 and other in NX9 same question, both (but what I realy need is to know if there is "turn off" option for that in nx 7.5). .... can´t upload images now (not woking)... will try later, just in case someone undersands what I am asking for.
1 REPLY

Re: turn off point coordinates en nx 75

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Guessing (due to lack of images)

If these dialogs "pop up" on the graphics window (seemingly 90% of time covering up something important you want to see), try hitting the "F3" button to toggle them off/on

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled