Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

ugtopv STANDALONE - OutputDirectory and MONOLITHIC seem not to work.

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi dear Experts,

I have discovered this issue, but I am very surprised that these 2 Options never worked, starting from NX5.

            (as far as I could test, at least).

            Maybe they worked fine on UG16,  but I do not have it anymore.

Nore : Input Assembly toycar_assy.prt is located in your NX install directory :

            <your_NX_dir>\UGOPEN\SampleNXOpenApplications\.NET\AssemblyViewer

 

 test05.jpg

 

COMMANDLINES :

@set PATH=E:\MultiNX\NX5\NX506\NX506_10;E:\MultiNX\NX5\NX506\NX506_10\UGII;%PATH%

E:\MultiNX\NX5\NX506\NX506_10\PVTRANS\ugtopv.exe .\toycar_assy.prt -config=.\tessUG_05.config -generate_assy_jt

 

ISSUE :

On NX09, 10, 11 and 12 the result of STANDALONE (PRTs on disk) ugtopv is always a mimic bunch of single JT files in the current directory where I launch the bat file !!! Not correct.

Reproduced also on NX 8.5 , 7.5.5 and 5.

 

 

ISSUES Details :

  • OutputDirectory is not honored
  • MONOLITHIC is not honored

 

Here the main interesting Options which I used in the tessUG.config :

 

            OutputDirectory = "C:\JT-Files_05_batch\"

            CommonPartsPath = ""

            chordalOption = "RELATIVE"

            structureOption = "MONOLITHIC"

 

Thanks in advance if you have got any explanation or experience.

 

Enzo

1 REPLY 1

Re: ugtopv STANDALONE - OutputDirectory and MONOLITHIC seem not to work.

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

-honour_structure commandline option was the solution.

 

Enzo