Cancel
Showing results for 
Search instead for 
Did you mean: 

use of expression for scaling the model

Experimenter
Experimenter

how can i use expression for scaling the model.

suppose i have one body which is to be scaled down or up depending on certain ratio.

I want to use expression for this so that my body remains parametric after parametric.

can anyone help me with this.

5 REPLIES 5

Re: use of expression for scaling the model

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @RC41805,

With 'Scale Body' command, scale factor can be specified using expression. Did you try it?

Re: use of expression for scaling the model

Experimenter
Experimenter

i am new to this can you explain me in detail.

actually i want to automate the process by using expression

Re: use of expression for scaling the model

Siemens Phenom Siemens Phenom
Siemens Phenom

Here is a example

(view in My Videos)

Re: use of expression for scaling the model

Experimenter
Experimenter

Thanks for the answer Ganesh.

 

But i want only want some dimension to change like i don't hole,fillet radius to be change and want body to be parametric 

 

like if i have 15 dimension, i want to scale only 10 dimension by using certain ratio

Re: use of expression for scaling the model

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

then I would

- use expression editor to create the scale expression

- modify each feature, multiply the appropriate parameters by that expression

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled