Cancel
Showing results for 
Search instead for 
Did you mean: 

vertical weld symbol

Pioneer
Pioneer

Hi

Is possible in NX8.5 create vertical weld symbol instead horizontal in the Drafting? I can only reverse direction of the stub line.

 

5 REPLIES

Re: vertical weld symbol

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @MartinReiter,

After creating the weld symbol, you can rotate it by 'Move Object' (Ctrl+T) command.

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: vertical weld symbol

Pioneer
Pioneer

Yes, I tried it, because as I remember "Transform" worked in NX2. In NX8.5 I can rotate only text, not whole weld symbol (stub line stayed on the original position)

 

Re: vertical weld symbol

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Using Move Object to rotate a weld symbol works in NX 9+, but was a problem in 8.5.  

Re: vertical weld symbol

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
What happens if you edit the weld symbol and delete the leader? You should be able to use Move Object to rotate the entire remaining symbol and then reapply the leader.

Re: vertical weld symbol

Pioneer
Pioneer

Excellent!!! It works.

Thank you