Cancel
Showing results for 
Search instead for 
Did you mean: 

wave links not updated automatically in the assembly

Legend
Legend

Hello

I have a problem in assembly that I have seen many times. I have a linked body in a component. When I edit something in this component the linked body inside the component does not update. I must edit the link manually and deselect the original body and select it again to update the link. 

I attached a movie to show you the problem. in the active component I have a link to hollow box which is not updated. I just edit the link and deselected the hollow box solid body and select it again to update it.

Updating the links manually takes time and I am always worried about links which may be not update. 

I am sure all components are fully loaded (not partially) and my links are associative.

(view in My Videos)

12 REPLIES

Re: wave links not updated automatically in the assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi robot139,

 

You need to toggle the Delay Interpart Update off.

 

Best Regards

Fred

 

2018_11_21_11_00_42_NX_11_Modeling_model3.prt_Modified_.png

Re: wave links not updated automatically in the assembly

Legend
Legend

Thanks Sandman.

But it was already off.

I didn't know this option and had never changed it before. It was in its default status.

Regards.

Re: wave links not updated automatically in the assembly

Phenom
Phenom

What is the Load Statusof your Linked Components?

Re: wave links not updated automatically in the assembly

Legend
Legend

as I mentioned all components are fully loaded.

Re: wave links not updated automatically in the assembly

Siemens Genius Siemens Genius
Siemens Genius

Is the option Load Interpart Data turned on in your load options?  this will load the additional data needed to update the WAVE links

 

Keith

Re: wave links not updated automatically in the assembly

Legend
Legend

Nop! It was off.

I think this may solve my problem. I will check.

Thank you very much KeithWilson.

Re: wave links not updated automatically in the assembly

Siemens Genius Siemens Genius
Siemens Genius

With this option on, then your parts should update when loaded... not always a desired behaviour...

 

In general for WAVE workflows, 

 

1. Load Interpart Data ON

2. Delay Interpart Update ON

 

In this way you can control when your parts update rather than just having it happen at load

 

Keith

Re: wave links not updated automatically in the assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi robot139,

 

Strange, you say that you have been working in both parts - the wave link source part and the target part. This means that your parts should be fully loaded. Is your link going drirect from source to target or via another part? This would then be solved by having all parts contributing fully loaded. You can do that as a pre setting or while in the session use:

 

2018_11_21_13_05_05_NX_12_Modeling.png

Re: wave links not updated automatically in the assembly

Legend
Legend

I thought fully loading the components is enough.

Thanks a lot again.