Cancel
Showing results for 
Search instead for 
Did you mean: 

weld

Builder
Builder

Hello@ NX experts,

 

i have query in NX 11.0.2,

 

i cant find weld option in new version,,like groove weld etc in modeling.....

 

is there any change in version....

 

Thanks

Warm Regards
Thomas Roman
Machine Designer
5 REPLIES

Re: weld

Phenom
Phenom

Hi @Thomas_Roman,

have you installed MP 00 for NX 11.0.2 ? Thay have missed on NX 11.0.2 the weld application Smiley Happy

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

Re: weld

Builder
Builder
hello@cubalibre00

understood buddy,,

we can understand them,,,developers are also humans,,,

again thanks for the help buddy, appriciated for your help
Warm Regards
Thomas Roman
Machine Designer

Re: weld

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi cubalibre,

Thanks for the heads up.... yes weld assistant works with the mp00. Checked it sometime back on one of my friends system....however we were not able to use command finder to find out the weld assistant commands.... over to the experts...

@BenBroad: Hi Ben...can you please validate the same.. I do not have access to NX11.0.2 MP00 right now.

Best Regards

Kapil

Re: weld

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @kapilsharma,

 

Command finder is working for me and finding WA commands in NX11.0.2 mp0.  I was just validating the basic commands on the WA ribbon, is there a specific command you want me to try?

 

Regards, Ben

Re: weld

Siemens Phenom Siemens Phenom
Siemens Phenom
Thanks Ben...it might be an installation glitch then...we tried fillet/groove weld in the command finder.
Thanks and Best Regards
Kapil