Cancel
Showing results for 
Search instead for 
Did you mean: 

where to find the download link of the latest Patch of NX 10

Valued Contributor
Valued Contributor

Hello community,

 

 

yesterday a member of the maintenance staff called me back to help me with our issues. He soon noticed that we use an older Patch version.

We have NX 10.0.3.5 Patch None

He then sent me the link to the latest MP .

Unfortunately he sent us the link to nx-10.0.2.mp10.zip

I would have expected the file nx-10.0.3.5.mp10.zip (or what the latest Patch ever might be)

 

Since that person is not responding to my assumption that he sent us the wrong link I'll ask here:

Where can I find the correct Patch version.

 

 

Many thanks for your help.

 

 

 

5 REPLIES

Re: where to find the download link of the latest Patch of NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: where to find the download link of the latest Patch of NX 10

Valued Contributor
Valued Contributor

Many thanks for your support.

 

However, I don't understand why there is a nx-10.0.2.mp10.zip from Nov. 21, 2016

And there is a nx-10.0.3.mp10.zip from Nov. 2, 2016

 

When I look in Help/ About NX 10.0.3.5 and then in System Information I get

NX Version 10.0.3.5

NX Phase 5

NX Patch None

 

Patch is None, as it reads.

 

Why I don't find a Patch for that version?

What is the latest Version with the least bugs? 

 

Many Thanks for you help!

 

Best Wishes

Re: where to find the download link of the latest Patch of NX 10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX 10.0.3 MP10 is the latest release for NX 10.0.3 and it was released before NX 10.0.2 MP10.

The releases of MPs are not in order for older MRs.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: where to find the download link of the latest Patch of NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Blendy,

 

Just to clarify some stuff.

 

First of all, version 10.0.3.5, is the same as 10.0.3. The last number, phase 5, is just for internal releases. so you can ignore that bit. It's more for us, GTAC and development, so we can check a customer did not exidently used a beta, or pre-released version.

 

About the dates of MP's.... Since the latest mainenance release is the release development focuses. So there are more MP's released for NX 10.0.3 that their are for NX 10.0.2.

 

There is a slight chance that MP10 for 10.0.2 contains a fix that is not yet included in MP10 for 10.0.3. But if this is the case, this bugfix will will also go in MP11 for 10.0.3. But at the same time, there are a lot of bug fixes for MR 10.0.3 AND MP10 that did not go into 10.0.2 and that MP10. So if you want the most issues to be fixed, go for NX 10.0.3 MP10.

 

I hope this clears it a bit.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: where to find the download link of the latest Patch of NX 10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Blendy wrote:

 

Unfortunately he sent us the link to nx-10.0.2.mp10.zip

I would have expected the file nx-10.0.3.5.mp10.zip (or what the latest Patch ever might be)


I'm guessing he accidentally picked the wrong link.

Note that MPs are specific to the specified MR (maintenance release).

I.e. "nx-10.0.2.mp10.zip" sould ONLY be applied to NX10.0.2 (NOT to 10.0.3, NOT to 10.0.1, NOT to 10.0.0)

"nx-10.0.3.5.mp10.zip" should ONLY be applied to NX10.0.3

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled