Cancel
Showing results for 
Search instead for 
Did you mean: 

why am I always loosing link body when opening a big assembly ?

Pioneer
Pioneer

Hi ! each time I am opening an assembly I am having linked part that are not showing.... any clue on how to stop this issue ? thanks

10 REPLIES 10

Re: why am I always loosing link body when opening a big assembly ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Assuming it is native NX.

Does parts/components that are linked to the assembly resides in the different folder/directory?

Re: why am I always loosing link body when opening a big assembly ?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Is it that the part is not loading, or just not displaying?  When you open your assembly do you get a dialog listing parts that failed to load, or is there some other message reported?

Re: why am I always loosing link body when opening a big assembly ?

Pioneer
Pioneer
No they are stored in the same folder and directory part and assembly, all together and thay are native NX. thanks

Re: why am I always loosing link body when opening a big assembly ?

Pioneer
Pioneer

I always save in the same folder and never move the files... see the error message I haveunloaded.jpg

Re: why am I always loosing link body when opening a big assembly ?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

What happens if you change your Assembly Load Options to load "As Saved"?

 

Select "Menu > Information > Assemblies > List Components".  It should list the directory path for the file it failed to find: 2017_011_CV_V2b.prt.  Is it the same directory as the assembly?

Re: why am I always loosing link body when opening a big assembly ?

Siemens Phenom Siemens Phenom
Siemens Phenom

This may happen if you rename a component at OS level and open an assembly that has the renamed component.

Re: why am I always loosing link body when opening a big assembly ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Pdmartin,

 

I suspect that the part you are failing to load is not saved with the assembly so:

 

1. Ensure that the part causing the warning message resides in the Assembly

2. Load the part causing the issue manually

3. Ensure that all the assembly nodes all the way from the part causing the issue all the way to the top node is loaded fully

4. Save the assembly with the top node as Work Part - this will save all the assembly nodes recorrding your part to truly be part of your assembly, should there have been a glitch somewhere during creation & first save.

 

This should reslove your issue.

 

Best Regards

Fred

Re: why am I always loosing link body when opening a big assembly ?

Experimenter
Experimenter

PLEASE CHECK THE ASSEMBLY LOAD OPTIONS.

 

FILE>OPTIONS>ASSEMBLY LOAD OPTIONS.

 

LOAD - SHOULD BE 'FROM FOLDER'

Re: why am I always loosing link body when opening a big assembly ?

Pioneer
Pioneer
"as saved" - is better

Сhannel for NX users (Russian language) https://www.youtube.com/channel/UCvf0Rp4Sy6bRRyTYBF9rnJQ